Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
I Have ATV212 and it shows an error EPHO , how to solve this ?
EPHO means  [Output phase loss fault] :  Loss of one or more output phases

Solution :
• Determine the cause of the missing output phase (such as a bad connection, an output disconnect, or an open winding in the motor) and rectify the trouble.
• Check parameter F605.

F605 :Output Phase Loss  (attached)

Schneider Electric Egypt and North East Africa

Attachment(s)
F605 error.pdf [57.9 KB]