Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to solve OCF error in ATV32 ?
OCF it is an Overcurrent error

The causes may it be :
• Parameters in the [SETTINGS] (SEt-) and [MOTOR CONTROL] (drC-) menus are not correct.
• Inertia or load too high.
• Mechanical locking.

The solution:
• Check the parameters.
• Check the size of the motor/drive/load.
• Check the state of the mechanism.
• Decrease [Current limitation] (CLI).
• Increase the switching frequency.