Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
I have ATV71 with Error SCF1 , what is that error and how to solve it ?
SCF1 to SCF5 is a  Motor short-circuit fault

The causes could be :
• Short-circuit or earthing at the drive output
• Significant earth leakage current at the drive output if several motors are connected in parallel

To Solve it
• Check the cables connecting the drive to the motor, and the insulation of the motor.
• Reduce the switching frequency.
• Connect chokes in series with the motor.