Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are Line Reactors required on an ATV212 Drive?

Issue:
Do ATV212 drives need line reactors?

Product Line:
Altivar ATV212

Environment:
All model numbers

Cause:
None

Resolution:
No, line reactors are not required nor recommended for ATV212.

Data Bulletin 8800DB0702R06/11 Reduced Harmonics Technology in Altivar 212
The Altivar 212 adjustable speed drive, designed specifically for pump and
fan applications, has a unique and effective approach to reducing
harmonics called reduced harmonics technology (RHT). The Altivar 212
drive offers a unique, optimized power section and a powerful motor control
method that significantly reduces harmonic currents. The Altivar 212 drive
reduces harmonics by 60% or more without the use of additional harmonic
reduction devices.

AC line reactors are often used when the incoming AC line power is above
voltage specifications to reduce the effect of high line voltage. Adding a line
reactor will not significantly reduce or add to the Altivar 212 drive’s THDI.

Schneider Electric Egypt and North East Africa

Attachment(s)
8800DB0702.pdf [119.77 KB]