Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What materials are used for the Magelis XBTGT6330/GT6340 housing?
Issue:
What materials are used in the Magelis XBTGT6330/GT6340 housing?
Product Line:
XBTGT6330, XBTGT6340, XBTGT
Environment:
Physical Human Machine Interface (HMI)
Resolution:
Below are the materials used in the Magelis XBTGT6330/GT6340 targets:
Part Name         Material      Flame Resistance
Front Sheet        PET                 UL94 VTM-2
Front Bezel        ADC12
Rear Cover        PC/PBT           UL94 V-0