Issue
This Resolution explains a firmware compatibility issue with the BMXNOE0110 at PV11.
Product Line
BMXNOE0110
Resolution
Component obsolescence required a replacement part for the BMXNOE0110's. Modules with the new flash component are identified as PV11, which resulted in a new firmware version 5.9.
This Resolution explains a firmware compatibility issue with the BMXNOE0110 at PV11.
Product Line
BMXNOE0110
Resolution
Component obsolescence required a replacement part for the BMXNOE0110's. Modules with the new flash component are identified as PV11, which resulted in a new firmware version 5.9.
- BMXNOE0110's at PV11 or higher are only compatible with firmware versions 5.9 or higher.
- BMXNOE0110's at PV11 or higher cannot be downgraded with firmware versions lower than v5.9.
- BMXNOE0110 firmware version 5.9 and higher are compatible with all BMXNOE0110 PV versions.
Released for: Schneider Electric Egypt and North East Africa