Issue
Register List for ION7650 IEC61850 protocol
Product Line
ION7650
Environment
61850 Template on the device.
Cause
No register list for the IEC61850 protocol comes with the device.
Resolution
The IEC61850 register listing is defined in the IEC61850 standard. It is a proprietary register list of IEC. Therefore we cannot distribute the register listing for the IEC61850. To obtain the register listing the IEC61850 article would need to be purchased from IEC. The IEC61850 article lists the register mapping.
Register List for ION7650 IEC61850 protocol
Product Line
ION7650
Environment
61850 Template on the device.
Cause
No register list for the IEC61850 protocol comes with the device.
Resolution
The IEC61850 register listing is defined in the IEC61850 standard. It is a proprietary register list of IEC. Therefore we cannot distribute the register listing for the IEC61850. To obtain the register listing the IEC61850 article would need to be purchased from IEC. The IEC61850 article lists the register mapping.
Released for: Schneider Electric Egypt and North East Africa