Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Could you please confirm that the RACK-8800-RAW option (19” Essailec rack) can hold 2 x ION8800? The manual doesn’t explicitly say so.
The manual doesn’t explicitly say, however there are pictures presenting the dual-rack;

The part “RACK-8800-RAW” – rack for ION8800 - can hold 2 meters and it comes with 2 sets of Essailec connectors.

Rack Rack for two meters Two meters in one rack