Issue:
What communication options are available on the ATV12?
Product Line:
ATV12
Environment:
ATV12
Cause:
Network communications options
Resolution:
The ATV12 only has the modbus communication protocol available. A third party gateway can be used for other protocol of customer's choice.
What communication options are available on the ATV12?
Product Line:
ATV12
Environment:
ATV12
Cause:
Network communications options
Resolution:
The ATV12 only has the modbus communication protocol available. A third party gateway can be used for other protocol of customer's choice.
Released for: Schneider Electric Egypt and North East Africa