Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Does the ATV312 drive come with a remote keypad?

Article available in these languages: Spanish

Issue:
Is a remote keypad come with the ATV312 drive as standard?

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
The ATV312 drive does not come with a remote keypad as a standard item.  It must be ordered separately.
Remote Keypad Display
(IP54) ATV312, ATV12 VW3A1006
(IP65) ATV312, ATV12 VW3A1007
Mounting Kit, VW3A31101
Graphic Display  (used also with ATV61 and ATV71)  VW3A1101