Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause Err1 on ATV212 or ATV21 drive?

Article available in these languages: Dutch

Issue:
What can cause Err1 on ATV212 or ATV21 drive?

Product Line:
ATV212
ATV21

Environment:
All environments

Cause:
Setting the Refrences to the same number

Resolution:
This is a Speed Reference Fault.  It indicates an incorrect setting in F201, F202, F203, F204 OR F210, F211, F212, F213.

Verify these parameters, and set them properly.
Default settings are:
F201 = 0%
F202 = 0Hz
F203 = 100%
F204 = 50/60Hz

F2010 = 0%
F2011 = 0Hz
F2012 = 100%
F2013 = 50/60Hz

Schneider Electric Egypt and North East Africa