Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will cause the ATV212 drive not to start when the run contact between P24-F is closed?
Issue:
The ATV212 drive does not to start when the run contact between P24-F is closed.

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
When closing the run contact to logic input F, the VFD displays 0.0Hz.

Resolution:
- Verify that CMOd is set to 0 for terminal control.
- If any network functions are activated for monitoring purposes, set F108 = 48.
- Check your logic input programming.  Typically F111 = 2 for run forward function.  Other possibilities may combine run forward with other functions.
- Verify that the VFD is in Remote Mode.  The keypad LOC/REM button green LED should be OFF.
- Verify the VFD 24Vdc power supply by measuring P24 - CC.
- Check that the run circuit is complete by measuring for 24Vdc on F - CC.
- Verify that the VFD has a speed reference.  It may be running at 0Hz, indicated by a red RUN LED in the display.
- Verify whether the run permissive is being satisfied. If the drive displays "OFF", then the run permissive isn't satisfied. However, "OFF" is a normal state if the run permissive is activated when the run command is given.

Schneider Electric Egypt and North East Africa

Attachment(s)
atv212_programming_manual_en_s1a53838_02.pdf [3.58 MB]