Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the line or load reactor part number for a 480VAC. 25 hp drive?
Issue:
Line or load reactor part number for a 480VAC. 25hp drive.

Product Line:
ATV Drives

Environment:
All serial numbers for ATV Drives

Cause:
N/A

Resolution:
RL03503 for the Open Style
RL03513 for the Enclosed Type 1 rating