Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the thermal derating of Domae MCBs?
Are there any difference between the reference/standard temperature for Acti 9 and Domae MCBs?

Unlike Acti 9 MCBs (tested at 50°C), Domae MCBs are tested at 30°C. The derating tables for this range can be found attached.

Schneider Electric Egypt and North East Africa

Attachment(s)
Domae Derating and characteristics.xls [27 KB]