Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the EM3500 meter have built in phase loss detection?
Issue
Certain applications call for a simple device that can detect phase loss and notify a user of the alarm.

Product Line
EM3502(A), EM3550(A), EM3555, EM3560(A)

Environment
Power Monitoring, Basic Energy metering, Phase Monitoring

Cause
Application calls for a device that can alarm on phase loss without complicated programming.

Resolution
EM3500 series meters contain a dedicated phase loss alarm. This is in the form of a normally closed (NC) contact as well as an LED indicator on the front display.
NC contact is 30VA/C D/C MAx
This alarm output is in addition to any additional energy pulsing or digital outputs supplied with the meter.

Schneider Electric Egypt and North East Africa