Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME 7.2.2 - Archiving a database within database manager produces an error dialog stating 'Could not deploy package. Missing values for the following SqlCmd variables:LogFilePath

Issue:
Archiving a database within database manager produces an error dialog stating 'Could not deploy package. Missing values for the following SqlCmd variables:LogFilePath
Archive Database error in Database Manager in PME 7.2.2

Product Line:
Power Monitoring Expert 7.2.x

Environment:
Database Manager

Cause:
If the user chooses to save the archived database to the root of a directory - for example C:\, this error dialog will be displayed.

Resolution:
To workaround this, change the save location to a directory within a driver, say C:\Archives.

Additional Note:
The problem with saving an archive to the root of a directory was fixed for PME 8. However, you will still have a problem if you use the 'New ION Database' feature in Database Manager to create the new ION_Data database to the root of a drive. The resolution is to save to a directory. There are no plans to address this problem.

Schneider Electric Egypt and North East Africa