Search FAQs
How can I set up an ATV61/71 Drives to run reverse using Ethernet IP with assemblies 103 and 104?
Issue:
Setting up ATV61/71 drives to run reverse using Ethernet IP with assemblies 103 and 104?
Product Line:
Altivar ATV61 and ATV71 with Ethernet IP card VW3A3316
Environment:
All
Cause:
Needs to write a reverse command over the network using assemblies 103 and 104.
Resolution:
Ethernet IP command for REV using assemblies 103 and 104.
Reverse mode
bits 1, on
bits 5 on
bits 13 on
all need to be on
bit 4 needs to be off
or DEC 8226 is REV
Setting up ATV61/71 drives to run reverse using Ethernet IP with assemblies 103 and 104?
Product Line:
Altivar ATV61 and ATV71 with Ethernet IP card VW3A3316
Environment:
All
Cause:
Needs to write a reverse command over the network using assemblies 103 and 104.
Resolution:
Ethernet IP command for REV using assemblies 103 and 104.
Reverse mode
bits 1, on
bits 5 on
bits 13 on
all need to be on
bit 4 needs to be off
or DEC 8226 is REV
Released for:Schneider Electric Egypt and North East Africa
Explore more
Explore more