Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
could we replace the internal Bypass contactor for ATS22 with the external one to do the same function?
Unfortunately the ATS22 doesn't have the option to install an external by-pass contactor.

For example ATS48 have the relay (R2) wich gives the end of starting signal for the external bypass contactor.

So if the internal bypass contactor is defected, it is better to be replaced by a special order.