Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
I want the equivalent for SIRIUS SOFT STARTER SIEMENS P/N: 3RW4026- 1BB14, S0,25A,11KW/400V,40 DEGR.,AC200- 480V,AC/DC 110-230V,SCREW TERMINALS
Schneider equivalent soft starter is ATS01N232QN (SOFT-START STOP 32A  380 415V)