Issue:
Preset speeds set up for an ATV12.
Product Line:
ATV12
Environment:
All
Cause:
Installation / Setup
Resolution:
Set desired logic input (LIx) to PS2 in the FUN menu under PSS (Preset Speed) , then set SPx = desired speed. Note: you must be in terminal mode operation and low speed (LSP) will be the 1st preset speed.
Preset speeds set up for an ATV12.
Product Line:
ATV12
Environment:
All
Cause:
Installation / Setup
Resolution:
Set desired logic input (LIx) to PS2 in the FUN menu under PSS (Preset Speed) , then set SPx = desired speed. Note: you must be in terminal mode operation and low speed (LSP) will be the 1st preset speed.
Released for: Schneider Electric Egypt and North East Africa