Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find a list of ATV61 and ATV71 spare parts bulletins?

Article available in these languages: Spanish

Issue:
Spare parts bulletins list for ATV61 and ATV71.

Product Line:
Altivar ATV61 and ATV71 drives

Environment:
All

Cause:
Needs a spare parts bulletin for the ATV61 and ATV71 drives

Resolution:

https://www.se.com/us/en/download/
Enter the Bulletin# at the link above.

ATV61/71 Spare Parts Bulletins
DescriptionBulletin #
115v Logic Input Interface Kit30072-451-47
Conduit Entrance Kits (Nema 1) Size 2-8 30072-451-74
Conduit Entrance Kits (Nema 1) Size 9-13 30072-451-73
Control Terminal Board30072-452-06
Fan Kits (size 2 & 3)30072-452-08
Fan Kits (size 4 - 5B) 30072-452-09
Fan Kits (size 6 - 8) 30072-452-10
Fan Kits (size 9) 30072-452-11
Fan Kits (size 10- 15) 30072-452-48
Flange Mount Kits 30072-451-31B
Main Control Board Kits30072-451-86A
Frame Size 2, 3, 4, 5A, 5B - Spare Parts 30072-453-27
Frame Size 6 Spare Parts 30072-452-72
Frame Size 7A Spare Parts 30072-452-73
Frame Size 7B & 8 Spare Parts300072-452-74
Frame Size 9 Spare Parts30072-452-75
Frame Size 10 Spare Parts 30072-452-77
Frame Size 11 Spare Parts30072-452-78
Frame Size 12 Spare Parts30072-452-79
Frame Size 13 Spare Parts30072-452-80
Frame Size 14A Spare Parts 30072-452-81
Frame Size 14B Spare Parts 30072-452-98
Frame Size 15 Spare Parts 30072-452-82

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center