Issue:
ATV212 Modbus RJ45 and the screw terminals pin outs
Product Line:
Altivar ATV212, Sflex 212 SFD212
Resolution:
See the attached file
RJ45 connector
Pin 4= + DB or D1
Pin 5= - DA or DO
Pin 8= com
Screw terminals
B= +
A= -
GND= common
SCR= shield
The complete Modbus manual for the ATV212 products is downloadable from this link: https://www.se.com/us/en/download/document/S1A53844/
ATV212 Modbus RJ45 and the screw terminals pin outs
Product Line:
Altivar ATV212, Sflex 212 SFD212
Resolution:
See the attached file
RJ45 connector
Pin 4= + DB or D1
Pin 5= - DA or DO
Pin 8= com
Screw terminals
B= +
A= -
GND= common
SCR= shield
The complete Modbus manual for the ATV212 products is downloadable from this link: https://www.se.com/us/en/download/document/S1A53844/
Released for:Schneider Electric Egypt and North East Africa