Issue:
Telefast base that is used with the BMEAHI0812 HART module
Product Line:
Telefast
Resolution:
The following Telefast base can be used with the BMEAHI0812 HART module:
ABE7CPA02
ABE7CPA03
ABE7CPA31
using the BMXFTA1522/3022 cable
Telefast base that is used with the BMEAHI0812 HART module
Product Line:
Telefast
Resolution:
The following Telefast base can be used with the BMEAHI0812 HART module:
ABE7CPA02
ABE7CPA03
ABE7CPA31
using the BMXFTA1522/3022 cable
Released for: Schneider Electric Egypt and North East Africa