Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does the speed increase so slow when using the ATV312 jog dial in local control?
Issue:
Speed increasing slow when using the ATV312 jog dial in local control.

Product Line:
ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
Turning the jog dial slowly causes a minute change in the speed increments. If the jog dial is continued to be turned quickly, the speed increment increases.