Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the "Life" (MTTF) of ATV61/71?

Issue:
"Life" (MTTF) of ATV61/71

Product Line:
All ATV61 and ATV71

Environment:
All models and serial numbers.

Cause:
None

Resolution:
The MTTF (Mean Time To Failure) varies based on the Drive's part number. Please refer to the attached Excel sheet.

Schneider Electric Egypt and North East Africa

Attachment(s)
MTBF for ATV 61 and 71 V 1.0.xls [898.5 KB]