Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Vijeo Designer support Modbus/TCP USB communications to the M580?
Issue:
Does Vijeo Designer support Modbus/TCP USB communications to the M580?

Product Line:
Vijeo Designer, Magelis XBTGK/GT, HMIGTO/GTU/STO/STU, Smart Box, Compact Box, Flex Box

Environment:
HMI to PLC communication

Resolution:
Yes. Modbus TCP USB driver on HMIs in Vijeo Designer has been validated with M580. It does requires Unity V8.0 or higher or any version of EcoStruxure Control Expert for M580 and Vijeo Designer v6.2 SP2.1 or higher. The USB port is located on the front of the M580 CPU just below the LED display.
The cable to be used has the part number BMXXCAUSBH045.