Issue
While using the RecipeDB with the factorycast HMI, exceeding the maximum number of tables will cause the module to fail, this was tested with an automatic SQL request.
Product Line
Factory cast HMI (WMY, NMW)
Resolution
The maximum number of tables should be limited to 6 with 50 variables of 2 octets per table to insure a stable system.
While using the RecipeDB with the factorycast HMI, exceeding the maximum number of tables will cause the module to fail, this was tested with an automatic SQL request.
Product Line
Factory cast HMI (WMY, NMW)
Resolution
The maximum number of tables should be limited to 6 with 50 variables of 2 octets per table to insure a stable system.
Released for: Schneider Electric Egypt and North East Africa