Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Using the ATV61 or ATV71 drives, which communication option cards allow you to view the drive through a web page?
Issue:
Webpage access with drive.

Product Line:
Altivar 61, Altivar 71

Environment:
All models and serial numbers

Cause:
Needs an option card that allows him to view an web page.

Resolution:
There were three option cards that allow web page viewing for ATV61 and ATV71.
VW3A3310D Ethernet TCP/IP card
VW3A3316  Ethernet IP card
VW3A3320 combo Ethernet TCP/IP and IP card

Schneider Electric Egypt and North East Africa