Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to setup the ATV61 or ATV71 HMI keypad to monitor two parameters other than frequency reference in hertz on the display screen?
Issue:
How to setup the HMI keypad to monitor parameters other than frequency in hertz on the display screen.

Product Line:
ATV61/71 Drives

Environment:
All serial numbers for ATV61/71 Drives

Cause:
N/A

Resolution:
To setup the HMI keypad to display parameters other than frequency in the displays screen follow these steps:
1.  In the main menu go to Menu 6 Monitoring Configuration.
2.  In the Monitoring Configuration Menu go to Menu 6.2 Monitor Screen Type: Example Digital.
3.  Then go to Parameter Selection.
4.  You can now choose up to 2 parameters.

Note: These parameters will be shown on the screen before the Main Menu.
Only 2 parameters can be choosing at a time.
displayed parameters

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center