Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What cables can be use to connect to a M221 from a PC over USB?
Issue:
Connecting to the M221

Product line:
M221 all controllers

Environment:
EcoStruxure Machine Expert Basic (formally known as SoMachine Basic)

Cause:
Connection issues

Resolution:
The programming cables that can be used to connect to a M221 over USB are the following;
TCSXCNAMUM3P or the BMXXCAUSBH045.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center