Issue:
PTFL fault on the ATV61 and ATV71 drives.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Drive is faulting on power up.
Resolution:
This is a PTC error fault. Check to see if the PTC switch is turned ON if so check to see if the PTC input is open or shorted.
PTFL fault on the ATV61 and ATV71 drives.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Drive is faulting on power up.
Resolution:
This is a PTC error fault. Check to see if the PTC switch is turned ON if so check to see if the PTC input is open or shorted.
Released for: Schneider Electric Egypt and North East Africa