Search FAQs
In Proworx 32, how can I be certain that the Project was downloaded to the PLC?
Issue
Proworx 32 project download confirmation
Product Line
Proworx 32
Resolution
Proworx 32 will post a "Write to PLC Complete" in Message Central if the write was successful (see attachment).
Proworx 32 project download confirmation
Product Line
Proworx 32
Resolution
Proworx 32 will post a "Write to PLC Complete" in Message Central if the write was successful (see attachment).
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: