Issue:
ATS48 conformal coated components
Product Line:
ATS48 series soft starts
Environment:
All models of ATS48 and ATS48XXXXXS338
Cause:
Information not available in current literature.
Resolution:
Standard ATS48 version has:
- most of the elements of control board coated (except relays, display, some capacitors)
- some of the elements (IC's and others) of power board coated.
This standard coating makes the ATS48 conformed to the environment standard: IEC 60664-1, Pollution Degree 3.
These unit are available in the United States
Special ATS48 version (you can order it by the reference with S338 at the end, ex.: ATS48C25YS338 ) has:
- enforced conformal coating.
This special ATS48xxxxS338 version conforms to: IEC60721-3-3 class 3C1 for aggressive ambience.
These units has NOT been released for sale in the United States
ATS48 conformal coated components
Product Line:
ATS48 series soft starts
Environment:
All models of ATS48 and ATS48XXXXXS338
Cause:
Information not available in current literature.
Resolution:
Standard ATS48 version has:
- most of the elements of control board coated (except relays, display, some capacitors)
- some of the elements (IC's and others) of power board coated.
This standard coating makes the ATS48 conformed to the environment standard: IEC 60664-1, Pollution Degree 3.
These unit are available in the United States
Special ATS48 version (you can order it by the reference with S338 at the end, ex.: ATS48C25YS338 ) has:
- enforced conformal coating.
This special ATS48xxxxS338 version conforms to: IEC60721-3-3 class 3C1 for aggressive ambience.
These units has NOT been released for sale in the United States
Released for: Schneider Electric Egypt and North East Africa