Issue
Major updated feature release with firmware v2.0.1
Product Line
PM5500 series
Environment
Firmware
Cause
Additional functionality provides the PM5500 series meter with more application abilities
Resolution
*Warning: Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.
With fw version 2.0.1 the following topics are now available with the PM5500 series meters:
New method for firmware upgrades (FTP Server)
Ethernet gateway functionality
Simple Network Management Protocol (SNMP) support
TCP/IP filtering
Updated PM5563 with optional remote display
Email on alarm
SNTP time synchronization
Redesigned and updated webpages
Note
- This is not the latest firmware. For installation instructions and firmware dowload link refer to FA299853
- The DLF3000 software cannot be used. See page 135 of PowerLogic™ PM5500 Series User Manual for procedure.
- View addendum 7EN12-0285-00 for more details.
Released for: Schneider Electric Egypt and North East Africa