Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set up the ATV12 drive for 3 wire control?
Issue:
3 wire control setup on an ATV12

Product Line:
Altivar ATV12

Environment:
All

Cause:
He has 2  momentary pushbuttons 1 NC for stop and 1 NO for start

Resolution:
Arrow down to the FULL menu enter
Arrow down to IO menu enter
find tCC enter and set this to 3C ( you will need to hold the enter button for 3 seconds before it will change from 2C to 3C)

Schneider Electric Egypt and North East Africa

Attachment(s)
Programming manual.pdf [9.6 MB]