How can we help you today?

What is the F10 fault on a TR Inverter/Charger?

Environment:

12V or 24V DC battery systems

Cause:

F10 indicates a high battery voltage condition:

Above 15.5 V on a 12 V system
Above 31 V on a 24 V system

This typically occurs when the batteries are wired incorrectly, or an external charging source is pushing the voltage too high.

Resolution

Verify the batteries are connected in the correct configuration for the system (12V or 24V).
Check for external chargers, alternators, or solar controllers causing over‑voltage.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.