Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to start an ATV312 drive using modbus for command?
Issue:
Start an ATV312 using Modbus

Product Line:
Variable Frequency Drives

Environment:
Applies to ATV312

Cause:
Customer is not able to start the drive using Modbus.

Resolution:
Suggested to follow the status chart and send the values to the command word in sequence Hex 6 then 7 then F  to Address 8501 (assuming there is no offset)

flowchart

Schneider Electric Egypt and North East Africa