Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
BMXFTW301 cable diameter
Issue
This Resolution provides the maximum diameter for the BMXFTW301 cable.



Product Line
BMXFTW301



Resolution
The maximum BMXFTW301 cable diameter is 9.5mm


The BMXFTW301 is a cable used with M340 I/O modules.  It has a 20 pin terminal block on one end and color-coded flying leads on the other end.




Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center