Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the M7 coil suitable to be used with the LC1S150M7?
Kindly note the following
1. We could not find the reference LC1S150M7(incorrect reference) in any of the document, We hope it should be LC1D150M7.

2. M7 is not a coil reference, it is just indicating the voltage level(220 VAC, 50/60HZ) of contactor or contactor coil. We have many coil references available in catalog with "M7" at the end and all can not be used with LC1D150M7. The coil reference will change depending upon frame size(power rating) and the specific coil part reference for different contactor are provided in catalog and it is recommended to use those coils only.

The coil reference LX1D8M7 is suitable for LC1D150M7 contactor and the same coil should be used for LC1D150M7 contactor. The datasheet for coil LX1D8M7 is attached herewith for your reference.

We believe the information provided above will clarify your query. Please feel free to contact us for any of further assistance.

Schneider Electric Egypt and North East Africa

Attachment(s)
LX1D8M7.pdf [53.03 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: