Issue
The customer wants to know what components are required to be installed prior to performing SPM/PME installation, and they also want to verify that all components were installed correctly during the process.
Product Line
Struxureware Power Monitoring 7.0
Power Monitoring Expert 7.2
Environment
Web Applications
Cause
Uninstalling, or missing components would cause some segments of the Web Application not to function properly.
Resolution
The following sections need to be installed prior to starting the SPM/PME installation:
i) Common HTTP Features
e) In addition, the followings are installed:
i) Application Development Features
The customer wants to know what components are required to be installed prior to performing SPM/PME installation, and they also want to verify that all components were installed correctly during the process.
Product Line
Struxureware Power Monitoring 7.0
Power Monitoring Expert 7.2
Environment
Web Applications
Cause
Uninstalling, or missing components would cause some segments of the Web Application not to function properly.
Resolution
The following sections need to be installed prior to starting the SPM/PME installation:
i) Common HTTP Features
- Static Content
- Default Document
- Directory Browsing
- HTTP Errors
- HTTP Logging
- Request Monitor
- Request Filtering
- Static Content Compression
- IIS Management Console
e) In addition, the followings are installed:
i) Application Development Features
- (1) ASP.NET
- .NET Extensibility
- (3) ASP
- (a) If prompted to add other role services, required by selections, click “Add Required Role Services”.
- (4) ISAPI Extensions
- (5) ISAPI Filters
- ii) Management Tools
- IIS 6 Metabase and IIS configuration compatibility
- IIS 6 WMI Compatibility
- IIS 6 Scripting Tools
Released for: Schneider Electric Egypt and North East Africa