Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Where is the enter or ENT button on the Altivar ATV61 and ATV71 drives when using the VW3A1101 HMI for programming?
Issue:
ENT button on ATV61/ATV71 when using the VW3A1101 HMI

Product Line:
Altivar ATV61 and ATV71 or any drive using the VW3A1101 for programming.

Environment:
All

Cause:
Need to know how to save the parameters after entering data into the drive.

Resolution:
The enter or ENT button is the large round knob on the W3A1101 keypad. Just push the wheel to enter.