Procedure on How to Use OPC Test Client
Issue
An OPC Client does not read values from the OPC Server provided by Power Monitoring Expert (PME). As such it is necessary to verify OPC Server is functioning properly. For this purpose, OPC Test Client, a utility provided by PME can be used.
Product Line
Power Monitoring Expert (PME)
Environment
OPC
Cause
Testing OPC Server capability of PME to verify its functionality.
Resolution
1. Run OpcTestClient.exe from ...\system\bin\ in PME installation folder.
2. Click on 'Connect' button on the right side.
Note that the OPC Server address (opcda://localhost/ION.OpcDaServer) is already selected in the 'Server' drop down list. If not, it should be selected from the drop down list:
Upon connection, ION.OpcDaServer will appear in the left pane:
3. Right click on ION.OpcDaServer and select 'Create Subscription...':
4. Provide a name for the subscription and click Next:
The devices will populate on the left side:
5. Select a measurement from a device. Double click on the tag to transfer it to the right pane:
6. Click Next:
7. Click Done to see the value:
Note* There is no link to OPC Test Client. It can be found in the installation folder created by the PME software.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.