Issue:
Set logic inputs other than LI1/DI1 for run forward command on an Altivar drive.
Product Line:
Altivar drives
Environment:
All
Cause :
LI1 logic input inoperative
Resolution:
In 2 wire control, LI1/DI1 is run forward. In 3 wire control, LI1/DI1 is stop and LI2/DI2 is run forward.
In either configuration, LI/DI1 must be active for the drive to run and no other inputs can be assigned as run forward.
Released for:Schneider Electric Egypt and North East Africa