Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to install BlokSeT IP54 under a shelter / shed or in a room where one side exposed to the atmosphere ?
No. We do not recommend installation of BlokSeT IP 54 under a shelter / shed or in a room where one side exposed to the atmosphere.
BlokSeT is tested and certified for Indoor application only.