Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum pulse length of my TM5SDI2DF TM5 module ?
Maximum pulse length depends on the chosen clock frequency:

Clock Frequency
Maximum Size of Pulse
48 MHz
1.3653125 ms
24 MHz
2.730625 ms
12 MHz
5.46125 ms
6 MHz
10.9225 ms
3 MHz
21.845 ms
1.5 MHz
43.69 ms
0.75 MHz
87.38 ms
0.375 MHz
174.76 ms
0.185 MHz
354.2432432 ms