Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to control an ATV61 / ATV71 with a M340 CPU built-in Ethernet port using the DATA_EXCH function
The attached document describes an application using a M340 CPU with a built-in Ethernet port connected to an ATV71 Ethernet card VW3A3310D and using the DATA_EXCH function. The M340 will be communicating with the IO Scanner service in the drive.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Attachment(s)
M340 and ATV71 using ModbusTCPIP and Data_Exch function.pdf [464.04 KB]