Issue:
Is ATV212 designed for or a constant torque application such as Positive Displacement Pump?
Product Line:
Altivar 212, S-Flex
Environment:
All models and serial numbers
Cause:
N/A
Resolution:
The ATV212 is designed for variable torque applications. A positive displacement pump is considered a constant torque application so the ATV212 is not recommended.
Is ATV212 designed for or a constant torque application such as Positive Displacement Pump?
Product Line:
Altivar 212, S-Flex
Environment:
All models and serial numbers
Cause:
N/A
Resolution:
The ATV212 is designed for variable torque applications. A positive displacement pump is considered a constant torque application so the ATV212 is not recommended.
Released for:Schneider Electric Egypt and North East Africa