Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Isolation clarification of ERIO communication modules
The ERIO communication modules include 140CRP31200 ,140CRA31200, BMXCRA31200 ,BMXCRA31200 and BMECRA31210.

These following properties can be applied to these modules
1: Isolation Voltage : 1500VAC between each ethernet ports
2: Isolation Voltage : 1500VAC between primary and secondary of ethernet port
3: The two device network ports operate in redundancy mode ,if one port fail or cable is disconnected in one port ,the communication between remote drop and head module will not be interrupted if the communication ring link is properly deployed.

Schneider Electric Egypt and North East Africa