Issue
How to install and setup the PowerLogic Tenant Billing custom page on an EGX300 Gateway
Product Line
EGX300 Ethernet Gateway
Environment
EGX300
Cause
Installation and setup instructions required to generate bills using the PowerLogic Tenant Billing custom page on an EGX300 Gateway not readily accessible.
Resolution
The setup guide to installing the EGX Tenant Billing solution, which is a pack of custom pages that can be added to the EGX to allow users to create logical tenants for which bills can be generated, is attached below.
Setup of the EGX Tenant Billing solution requires two steps. First the commodity_mappings.xml file must be configured for each device to be billed off. This is described in the Commodity Mapping Configuration section within the Setup Guide. Second, files must be placed in the monitoring folder of the EGX that the user wants to install the solution on. This can be achieved by manually moving the files to the EGX or by using the provided billing_upload.bat file. Both ways are described step by step below in the Batch File Setup section and the Manual Setup section within the Setup Guide.
For further instructions on configuring the Owner information, tenants, billing points, move in/out estimate and generating bills, refer to the PowerLogic Tenant Bill Overview guide attached below.
How to install and setup the PowerLogic Tenant Billing custom page on an EGX300 Gateway
Product Line
EGX300 Ethernet Gateway
Environment
EGX300
Cause
Installation and setup instructions required to generate bills using the PowerLogic Tenant Billing custom page on an EGX300 Gateway not readily accessible.
Resolution
The setup guide to installing the EGX Tenant Billing solution, which is a pack of custom pages that can be added to the EGX to allow users to create logical tenants for which bills can be generated, is attached below.
Setup of the EGX Tenant Billing solution requires two steps. First the commodity_mappings.xml file must be configured for each device to be billed off. This is described in the Commodity Mapping Configuration section within the Setup Guide. Second, files must be placed in the monitoring folder of the EGX that the user wants to install the solution on. This can be achieved by manually moving the files to the EGX or by using the provided billing_upload.bat file. Both ways are described step by step below in the Batch File Setup section and the Manual Setup section within the Setup Guide.
For further instructions on configuring the Owner information, tenants, billing points, move in/out estimate and generating bills, refer to the PowerLogic Tenant Bill Overview guide attached below.
Released for: Schneider Electric Egypt and North East Africa