Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can I do if the PLC TM221 reboots continuously after an update with firmware 1.3.2.1 SP1?
This issue can be solved by downloading any application in the PLC TM221 via USB in powerless mode (no power supply connected).
After that, the issue will not appear anymore.